Post Go back to editing

ADP1876 parallel operation

Category: Hardware
Product Number: ADP1876

Hi ,

ADP1876 is a switching regulator with two channels ,each can deliver to load upto 25A but the channels have 180 degree  phase shift , Is it possible to get 50A load current by combining both channels? If it is possible please let me know how do we do it

Thank You.

Parents Reply
  • Hi Aravind,

    The simplest way would be adding bleeder resistor to the output.

    You can also do a 4-phase operation by adding a multiphase oscillator like LTC6902 and connect the outputs to SYNC of each ADP1850. You can also simulate 4-phase operation in LTSpice with LTC6902 and ADP1850. Thanks!

Children
No Data