Post Go back to editing

thermal via layout for LTC3308A exposed pad

Category: Choose a category
Product Number: LTC3308A

Dear Sir,

I was asked about thermal via layout for LTC3308 exposed pad from our customer. According to the datasheet p18, recommended number of via and size is as below.

In the recommended layout, five 5mil vias are used to provide the best conductivity to the GND plane within the EPAD. For layouts where 5mil vias are not allowed, it is recommended to use either four 8mil vias or a single (filled or tented) 12mil diameter via.

I would like to know about recommended via size for 2 and 3 vias. Please advise.

Regards,

Koide

Parents Reply Children
  • Hi Marty,

    Thank you for your additional comment. Our customer is facing same situation, so they try to use 8mil vias but in trouble with solder wicking and connection problem. We would appreciate If you have any other case-study materials to prevent the problem.

    Regards,

    Koide

  • Hi Marty,

    Could you please advise about recommended dimensions for followings?

    - Land diameter for 5mil, 8mil and 12mil via.

    - Stencil thickness

    Also advise the stencil thickness for DC2991A, LTC3308A demo board.

    Regards,

    Koide

  • Hi Koide,

    Below is what I received from our layout engineer.

    I typically use the following dimensions for the start of the via and the end of the via for the via’s they are asking about:

     10/12 mil annular ring for a 5 mil drill

    14/16 mil annular ring for a 8 mil drill

    20/22/24 mil annular ring for a 12 mil drill.

    This is based on the boards and design rules we use. Other thicker boards with many layers and some designer rules do not allow for smaller via drill sizes.

    We didn't have any information on the stencils at the moment. 

    Regards,

    Marty

  • Hi Koide,

    I did find out that we always try to use 5 mils but if there are fine pitch leadless components (< 1mm) and BGAs etc., we’ll go for 4 mils. For the LTC3308A demo board we used 5 mils.

  • Hi Marty,

    Thank you for the answer for my question. Our customer try to use four 5 mils thermal vias, but due to their PCB supplier technical constraints, they plan to use 8 mils with some countermeasure for solder wicking so far.. I'll share the information from you with our customer. 

    Regards,

    Koide

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.