Post Go back to editing

thermal via layout for LTC3308A exposed pad

Category: Choose a category
Product Number: LTC3308A

Dear Sir,

I was asked about thermal via layout for LTC3308 exposed pad from our customer. According to the datasheet p18, recommended number of via and size is as below.

In the recommended layout, five 5mil vias are used to provide the best conductivity to the GND plane within the EPAD. For layouts where 5mil vias are not allowed, it is recommended to use either four 8mil vias or a single (filled or tented) 12mil diameter via.

I would like to know about recommended via size for 2 and 3 vias. Please advise.

Regards,

Koide

Parents
  • I do not know the answer for 2 or three vias. The thermal vias provide cooling for the part and also a needed GND connection. If the layout calculator is available to calculate the impedance of the vias for the board thickness, copper thickness, and via holes, the number of vias and the via size that provides the least impedance should be used. The LTC3308A is a 4 amp part and the GND connection along with the two PGND pins need to provide a good return path to the VIN caps to provide a short low impedance path in the hot loop (the AC switching currents). If the vias holes are large enough the solder past can wick away from the EPAD and provide a poor connection. With larger vias tenting or filling the vias might be required. 

Reply
  • I do not know the answer for 2 or three vias. The thermal vias provide cooling for the part and also a needed GND connection. If the layout calculator is available to calculate the impedance of the vias for the board thickness, copper thickness, and via holes, the number of vias and the via size that provides the least impedance should be used. The LTC3308A is a 4 amp part and the GND connection along with the two PGND pins need to provide a good return path to the VIN caps to provide a short low impedance path in the hot loop (the AC switching currents). If the vias holes are large enough the solder past can wick away from the EPAD and provide a poor connection. With larger vias tenting or filling the vias might be required. 

Children