Post Go back to editing

LT8391 does not Start

Category: Choose a category
Product Number: LT8391

Hello,

We've built 4 prototypes with 2 LT8391 stages. I've come across one that will not start, I've noticed the SS pin is a sawtooth (see waveform below). 

All input pins are appropriate levels: EN=5V, CTRL1,2=2V, PWM=5V, SYNCH=CLK (392KHz) - Also INTVCC=5V and VREF=2V.

The circuit is similar to the Evaluation Kit:

www.analog.com/.../DC2345A-5-SCH.PDF

Does anyone have any insight?

Edit: I neglected to also mention, there are no measured shorts in the FETs and LED output.

Edit Notes

Added additional context.
[edited by: Iain-Trakka at 12:07 PM (GMT -4) on 18 Aug 2022]
Parents Reply Children
No Data