| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | mpeters |
Closed |
LTM4650A
Recommended for New Designs
The LTM4650A is a dual 25A or single 50A output switching mode step-down DC/DC μModule® (micromodule) regulator with ±1% total DC output error. Included...
Datasheet
LTM4650A on Analog.com
LTC2971
Recommended for New Designs
The LTC2971, LTC2971-1, LTC2971-2, and LTC2971-3 are 2-channel high voltage Power System Managers used to sequence, trim (servo), margin, supervise, manage...
Datasheet
LTC2971 on Analog.com
Hi,
I am ADI DFAE of Anstek from Taiwan,
My customer has one application that is Vin=12V/ Vout=1.4V~1.6V (use program control output voltage) / Iout = 300A.
So we will use the LTM4650A + LTC2971 in this application.
We have two issue as following:
1. I don't find the application circuit data of 12-phase 300A in datasheet, Could you provide application circuit of 12-phase 300A for me ?
2. we use LTC2971 to Manage LTM4650A's output voltage, Is it suitable? If not, could you give us other suggestions??
If you have any issue, please let me know. Thanks!
Best Regards
Klex
Hi Klex,
I am an app engineer supporting LTM4650A. Thanks for your inquiry.
As for the application circuit of 12-phase 300A, totally 6x LTM4650A parts need to be used. Let's just call them U01, U02, ..., U06. For U01, it is in the similar role as U1 on Page 33 in LTM4650A datasheet, and for U02, U03, ..., U06, they are in the similar role as U2 on Page 33 in LTM4650A datasheet. You may use the identical design for most pin connections by referring to that page, except for the following ones:
To achieve the best possible interleaving and ripple cancellation effect, I recommend U01, U02, U04, U05's PHASMD pin be connected to GND, and U03's PHASMD pin be floated. At the same time, tie U01's CLKOUT to U02's MODE_PLLIN, tie U02's CLKOUT to U03's MODE_PLLIN, ..., tie U05's CLKOUT to U06's MODE_PLLIN. In this way, all 12 phases are 30 degree apart from each other.
Below is a picture to illustrate the above-mentioned point. This configuration is based on Page 15 in LTM4650A datasheet.
Feel free to let me know if you have any questions.
Best regards,
Zhengrong

Hi Klex,
I am an app engineer supporting LTM4650A. Thanks for your inquiry.
As for the application circuit of 12-phase 300A, totally 6x LTM4650A parts need to be used. Let's just call them U01, U02, ..., U06. For U01, it is in the similar role as U1 on Page 33 in LTM4650A datasheet, and for U02, U03, ..., U06, they are in the similar role as U2 on Page 33 in LTM4650A datasheet. You may use the identical design for most pin connections by referring to that page, except for the following ones:
To achieve the best possible interleaving and ripple cancellation effect, I recommend U01, U02, U04, U05's PHASMD pin be connected to GND, and U03's PHASMD pin be floated. At the same time, tie U01's CLKOUT to U02's MODE_PLLIN, tie U02's CLKOUT to U03's MODE_PLLIN, ..., tie U05's CLKOUT to U06's MODE_PLLIN. In this way, all 12 phases are 30 degree apart from each other.
Below is a picture to illustrate the above-mentioned point. This configuration is based on Page 15 in LTM4650A datasheet.
Feel free to let me know if you have any questions.
Best regards,
Zhengrong