Post Go back to editing

LTM4650A & LTC2971 application issue

Thread Summary

The user inquires about a 12-phase 300A application using LTM4650A and LTC2971. The final answer provides a configuration for 6 LTM4650A parts, with specific PHASMD and CLKOUT connections to achieve 30-degree phase interleaving. The accompanying answer suggests considering the LTC2972 or LTC3888 for managing the output voltage, but the user prefers to use the LTM4650A and LTC2971 due to stock availability.
AI Generated Content
Category: Hardware
Product Number: LTM4650A LTC2971

Hi, 

I am ADI DFAE of Anstek from Taiwan,
My customer has one application that is Vin=12V/ Vout=1.4V~1.6V (use program control output voltage) / Iout = 300A.
So we will use the LTM4650A + LTC2971 in this application.
We have two issue as following:
1. I don't find the application circuit data of 12-phase 300A in datasheet, Could you provide application circuit of 12-phase 300A for me ? 
2. we use LTC2971 to Manage LTM4650A's output voltage, Is it suitable? If not, could you give us other suggestions??

If you have any issue, please let me know. Thanks! 
Best Regards 
Klex



Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.