Post Go back to editing

Dynamic current limit adjustment using ADM1270

Category: Hardware
Product Number: ADM1270

Does anyone have experience in dynamically setting the current limit after start-up. For example using a DAC to control the voltage at ISET?

Is there anything I should be wary of?

For example according to the datasheet if ISET pin is connected to VCAP (3.6V), Vsense is set to the default of 50mV. However if ISET is avoltage lower than 3.6V typically through a resisitve divider, Vsense can be set from 12.5mV to 62.5mV. So by reducing the ISET voltage a higher limit (62.5mV) is actually also possible. 

Thanks for any suggestions