LTM8053 is rated at 3.5A continuous output current and 6A peak output current.
I need to know how long it can provide output at 6A (peak).
Can it remain producing 6A at more than 2 hours (for example)?
Thanks,
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTM8053
Recommended for New Designs
The LTM8053 is a 40VIN, 3.5A continuous, 6A peak step-down µModule® (power module) regulator. Included in the package are the switching controller, power...
Datasheet
LTM8053 on Analog.com
LTM8053 is rated at 3.5A continuous output current and 6A peak output current.
I need to know how long it can provide output at 6A (peak).
Can it remain producing 6A at more than 2 hours (for example)?
Thanks,
As I think you don't want add extra cooling this will not work. For 2h of 6A you should use two of LTM8053 or just a bigger module.
The mentioned peak rating belongs to the internal FETs capability and is purely intended for transient loads, With continuous use of 6A the part just gets too hot and will fail.

Check page 21, thermal considerations and the diagrams for the current derating over temperature.