Post Go back to editing

LT7182S Voltage Setpoint

Category: Hardware
Product Number: LT7282S

Hello,

I am designing a board with the LT7182S. I have two instantiations -- one instantiation where I combine VOUT0 and VOUT1 and set voltage to 2.0V, and another where I combine VOUT0 and VOUT1 and set voltage to 4.0V. Since the lookup table for the VOUTx_CFG resistor strap does not include 2.0V or 4.0V, my 'plan' is to set it to something 'close' via resistor strap, and then use the DC1613A PMBus pod to change the VOUT with LTPowerCAD.

However, ADI gives no particular procedure for changing VOUT0/1 via LTPowerPLAY.

To that end, I purchased the DC2836A EVM for the LT7182S and decided to see if I could figure out a procedure. HW-wise, I strapped VOUT0_CFG to 1.8V and set up a polyphase configuration. I also followed the reference design schematic notes to set up VOUT0 and VOUT1 in a parallel configuration. With VIN=12V, it powered up fine -- VOUT0 = VOUT1 = 1.8V and the POWERGOOD LEDs green. From there, I did the following:

1. Set the OPERATION register to 0x40 (soft power down), in both U0:0 and U0:1.

2. Set the VOUT field to 2.0V in the GUI for both U0:0 and U0:1.

3. Set the VOUT_MAX in the GUI to 2.1992V for both U0:0 and U0:1 (actually, one time it did this for me, the other time it didn't).

4. Powered up U0:0 and U0:1 --> the VOUT was 2.0V as expected.

Does it seem like a reasonable procedure?

Regards,
Mark

Parents
  • Hi Mark, 

    Thanks for choosing LT7182S in your design. Yes, your procedure all looks good. I am a bit surprised you saw one time failure while writing VOUT_MAX in the GUI to 2.1992V. If this keeps happening, please feel free to let us know. One note on the inductor selection just in case you have not made the change yet: the inductors of VOUT0 and VOUT1 channels are currently selected based on the 1.2V and 3.3V output voltage, respectively. If you are designing for single output channel with VOUT0 and VOUT1 tied together, please use two identical inductors instead of two different ones (e.g. 0.47uH and 1.2uH on the original DC2836A EVM board). This will give better performance for your design. 

    Thanks, 

    Haibo

Reply
  • Hi Mark, 

    Thanks for choosing LT7182S in your design. Yes, your procedure all looks good. I am a bit surprised you saw one time failure while writing VOUT_MAX in the GUI to 2.1992V. If this keeps happening, please feel free to let us know. One note on the inductor selection just in case you have not made the change yet: the inductors of VOUT0 and VOUT1 channels are currently selected based on the 1.2V and 3.3V output voltage, respectively. If you are designing for single output channel with VOUT0 and VOUT1 tied together, please use two identical inductors instead of two different ones (e.g. 0.47uH and 1.2uH on the original DC2836A EVM board). This will give better performance for your design. 

    Thanks, 

    Haibo

Children
  • Hi Haibo,

    Thank you for your reply. Regarding the inductor sizing, I should have also mentioned that I did modify the design with the proper inductor that I sized with the LTPowerCAD tool. (I tried to attach the LTPowerCAD design file to this message, but I got a "The file or URL is invalid" ... maybe it doesn't like the *.ltpc extension?)

    For the procedure I originally noted above, it worked. But that solution is volatile, so later I went on to come up with a procedure for making it non-volatile by committing it to the the EEPROM. I shorted VOUT_CFG0 and 1 to ground, because that is supposed to set VOUT to the value in the EEPROM, which is by default 0.5V. Actually, VOUT was 0V upon power up. I'm not sure why, but I was able to get it programmed properly. I think I'm good. I do have another question about it, but it's probably best to make another thread.

    Regards,

    Mark

  • Hi Mark, 

    Was the board set to polyphase configuration when you shorted VOUT_CFG0 and 1 to ground? If yes, both CH0 and CH1 would be "follower" and this may cause problem. If the SYNC/PWM_CFG was not configured as polyphase mode, I would expect both channels 0.5V after power-up. 

    Thanks, 

    Haibo

  • Hello Haibo,

    Yes, I had it set to Polyphase. See attached pdf for the modifications I made to the EVM.

    Regards,
    MarkPDF

  • Hi Mark, 

    The modification you showed here looks good and you will get 1.8V polyphase operation with 1MHz fsw. If you want default 0.5V output, only change R19 value to 0 Ohm and keep R20 to be 80.6k (80.6k sets fsw 1MHz, as shown in datasheet Table 4). If this does not give you 0.5V default output, please feel free to let me know. 

    Thanks, 

    Haibo 

  • Hello Haibo,

    Thank you for your help. I appreciate it.

    I went through my notes (I actually worked on this in the lab about a month ago), and I did indeed try shorting R19 to ground and I got the same vout result of ~0V.

    Regards,

    Mark

  • Hi Mark,

    Understood. Sorry that we did not respond in a timely manner. Apologize here. If there is further support I could provide on LT7182S, just post here anytime and I will receive immediate notification. 

    Thanks, 

    Haibo