Hello i have several questions about LT8722 :
- Is this component can be daisy-chain?
- Can we increase the efficiency at low load current (<1.5A)?
- Is there a minimum load current?
We have to regulate some TEC with these specifications :
- 3.3V max and 1.2A max
- 1.45V max and 0.8A max
- 3.8V max and 1.4A max
- 1.3V max and 1A max
Do you recommend to use LT8722, ADN8834 or LTM4663? We need to have a digital regulation with the best stability.