I made an evaluation board with LT8491 by myself.
It works, but it is hot very much.
I'm searching the cause of this heat.
Not the whole surface but the side of 33pin-52pin gererates heat, about 70 degree with 3 minutes.
This is saturated.
It's same as both with-load and without-load.
The circuit is blow.
I changed the FETs in red circle to the more drain current.
Could you give me some advices to solve ?

Edit Notes
Updated to ask a question new form[edited by: GenevaCooper at 1:14 PM (GMT -4) on 1 Aug 2022]