Hi Team!
I have gone through the Application Note 1120 Noise source in the LDO. I need to work the circuit on the 24V battery with automotive noise protection. I have used PI prefilter to increase PSRR mentioned in the AN. The values of the components used are as follows:
Lf = 10uF,
Cf = 22uF
Cd = 220uF
Rd = 1E.
To select the values of the filter, I have referred to the formula mentioned in the AN.
My question is I am enable to identify the power rating required for the resistor Rd.
Kindly help me to identify the power rating of the resistor Rd or formula to recognize the current flowing through the branch.
(The circuit used is from Fig 14 of the AN1120.).