Post Go back to editing

Which Voltage is applied to the gate of external NMOS from LT3751 IC?

Category: Datasheet/Specs
Product Number: LT3751

Hi everyone,

    I was trying to use the LT3751 IC but even when I replicate the schematic directly from the datasheet it didn't work. Then I read more in detail the datasheet and I got confused in the Voltage applied to the gate of the external NMOS because the gate driver operation says the gate driver has an internal, selectable 10.5V or 5.6V clamp but also the pin HVgate says the internal gate driver will drive the voltage to within VCC – 2V during each switch cycle and LVgate pin says depending of the connection the internal gate driver will drive the voltage to the VCC rail

Then, Which voltage is applied to the gate of external NMOS? 

Thanks for your help.