Hello Sir,
Please help see below schematic if can be design for LTC4231. Appreciate if you can feedback for any design related information.

LTC4231
Recommended for New Designs
The LTC4231 is a micropower Hot Swap controller that allows safe circuit board insertion and removal from a live power supply. An internal high side switch...
Datasheet
LTC4231 on Analog.com
Hello Sir,
Please help see below schematic if can be design for LTC4231. Appreciate if you can feedback for any design related information.

Hi,
The LTC4231 is not suitable for this application. The LTC4231 is a Micropower Hot Swap Controller for 1A or 2A applications as shown on the datasheet.
The main limitation of the LTC4231 is the limited gate driver. The Igate(up) is limited to 10uA (nominal) 7uA (minimum).
I suggest looking at the LTC4239.
JayBee