Post Go back to editing

What is the Vout max of the LT3045?

Category: Datasheet/Specs
Product Number: LT3045

Dear Sirs,

the LT3045 Datasheet on the title page in the Features section is showing: Output Voltage Range: 0V to 15V.
On the Demo Manual of the SCP-LT3045-1-EVALZ board it is reported that the LT3045 can supply an output voltage, maximum, of 19.5V.
I am confused: why on the Datasheet Vmax is 15V while the SCP-LT3045-1-EVALZ demo board provides 19.5V?
Could you kindly clarify the matter for me?

Thank you very much in advance for your kind reply.

Parents Reply Children
No Data