Post Go back to editing

DC1161B evaluation board Gain Phase margin plots and importing DC1161B evaluation into LTPowerCad

Category: Hardware
Product Number: DC1161B

Does anyone have manufactures Gain Phase margin data plots for DC1161B evaluation board, this board uses LT3507 buck regulator, the data sheet for the evaluation board doesn't show the performance specification for gain and phase margin ?

Also is there a reference LTspice schematic for the DC1161B that can be imported into LTpowerCad ?

Parents
  • Thanks for application of LT3507 buck regulator.

    Yes, we have the LTPowerCad that has the VB-programmed spreadsheet that can generate the bode plot of LT3507 based on the settings of the circuit.

    For DC1161B, the settings of the circuit can be set in the LTPowerCad spreadsheet to have all the detailed information.

    Best regards,

    Andrew

  • Thankyou, I have tried out the excel spread sheet within LTPowerCad which shows the bode plots for each channel for the LT3507. Do you know if the excel spreadsheet can be exported as a design file for use within the main LTPoerCad application, or is there a LTPowerCad design file for the DC1161B demo board that can be imported directly into LTPowerCad so as to make use of other features within the software application i.e. the the EMI filter calculator and other various plots which show on the main LTPowerCad application.

Reply
  • Thankyou, I have tried out the excel spread sheet within LTPowerCad which shows the bode plots for each channel for the LT3507. Do you know if the excel spreadsheet can be exported as a design file for use within the main LTPoerCad application, or is there a LTPowerCad design file for the DC1161B demo board that can be imported directly into LTPowerCad so as to make use of other features within the software application i.e. the the EMI filter calculator and other various plots which show on the main LTPowerCad application.

Children