I am designing a dimmable led streetlight rated for 215V at 0.7A. I was asking if I could use the lt3799 for my application. In the Data sheet it is rated for 40W-100W+. Can I use it for my 150W application?
LT3799
Production
The LT3799 is an isolated flyback controller with power factor correction specifically designed for driving LEDs. The controller operates using critical...
Datasheet
LT3799 on Analog.com
I am designing a dimmable led streetlight rated for 215V at 0.7A. I was asking if I could use the lt3799 for my application. In the Data sheet it is rated for 40W-100W+. Can I use it for my 150W application?
It's possible. LTspice model is available.
Thanks. I will use it.
Thanks. I will use it.