Post Go back to editing

DC\DC Boost 3.3V to 5V 200mA Max

Category: Hardware

I am looking for a DC\DC Boost regulator 3.3V to +5V Max 200mA (TYP : 50mA) with the smallest PCB area possible. We currently have a ADP2504 that takes a total PCB area of 7mm x 6mm. This is a little over kill in the current rating but we will use it unless I can find something close to half the area and is normally stocked. Do you have anything that could meet my requirements ? Also I can not go below a pitch of 0.5mm !

Parents Reply Children