Hello,
Can I have the references of the 3.3V regulator to be used in a direct connection between the LTC9101-1 and LTC9102? or other information.

Thanks.
LTC9101-1
Recommended for New Designs
The LTC9101-1/LTC9102/LTC9103 chipset is a 48-port power sourcing equipment (PSE) controller designed for use in IEEE 802.3at Type 2, 802.3bt Type 3 and...
Datasheet
LTC9101-1 on Analog.com
LTC9102
Recommended for New Designs
The LTC®9101-2/LTC9102 chipset is a 12/24-port power sourcing equipment (PSE) controller designed for use in IEEE 802.3bt Type 3 and 4 compliant Power...
Datasheet
LTC9102 on Analog.com
Hello,
Can I have the references of the 3.3V regulator to be used in a direct connection between the LTC9101-1 and LTC9102? or other information.

Thanks.
Hello,
The evaluation board uses LTC3639EMSE, a 150Vin / 100mA synchronous buck regulator from ADI.
The 3.3V regulator should be rated for at least 80V to handle input transients. The LTC9101-1's VDD max current draw is 60mA, and each LTC9102/LTC9103's CAP3 max current draw is 6.6mA. This means a system with one LTC9101-1 and four LTC9102/LTC9103s may draw a max of 86.4mA from a shared 3.3V supply.
Best Regards,
Eric
Hello Eric,
Thank you. This is exactly what I was looking for.
Regards,
Laure