Post Go back to editing

Replacing LTM4644 by LTM8060

Category: Hardware
Product Number: LTM8060, LTM4644

Hi,

Please refer to the link for understanding the issue that we are facing while using LTM4644.

Now we are planning to use LTM8060 by re-designing our board since our product is very much space constrained and cannot use LTM4644+ LDO based approach.

I would be very helpful if an FAE from Analog Device can share the noise spectrum of LTM8060 in dBm vs Frequency axis, like the way it was done in this link's suggested answer.

It would be better if test conditions are as below or something similar that would reflect the below condition.

Test Condition - 1

Vin=12V

VOut1 - 3.3V at 1A, Vout2 - 1.3V at 2A, Vout3 and Vout4 - 1.3V at 5A

Test Condition - 2

Vin=12V

VOut1 and Vout2 - 1.3V at 5A, Vout3 - 1.3V at 2A and Vout4 - 1.8V at 1A

Parents Reply Children
No Data