Post Go back to editing

LT3999 RT Pin

Category: Hardware
Product Number: LT3999

Dear experts,

I would like to know if it is possible to change the Rt=49,9kOhm - recommended value by the datasheet - to reduce the base bias current and all over the quiescent power consumption of the device? My application uses a simple push pull architecture which has a 18mA current consumption in no load (which of course include transformer, diodes etc losses..)

Thanks and regards,

Andras Magyar