Hello!
I made a high power DC/DC converter and the mosfet TG1 doesn´t open, the waveform Vgs is:
zooming:
and the Vg refered to ground (blue) and sw1(ellow) node is:
The bst capacitor is charged to 3v only
what can be the problem?
Hello!
I made a high power DC/DC converter and the mosfet TG1 doesn´t open, the waveform Vgs is:
zooming:
and the Vg refered to ground (blue) and sw1(ellow) node is:
The bst capacitor is charged to 3v only
what can be the problem?
Hi,
Have you tried checking/simulating your design in LTSpice? Please check your converter for possible cold solders and double check your circuit connection.
Regards,
Jhun
All of these issues are checked and the problem still the same. Any other problem that can cause this?
Also changing the bst capacitance doesnt solve the problem.
Are you using the demoboard or this is your self designed PCB?
Regards,
Jhun
is self designed, triying to follow the demo board.
regards.
Try getting a demoboard for the LT8390-1 and try converting it to your design. It can help you debug your problem. If the simulation is working as intended and there are no cold solders and you have the right components, it might be a PCB problem.
Have you tried changing your MOSFETs/IC to check for failure?
Regards,
Jhun
It might also help if you check the PGOOD pin to see if you are hitting any protection.
Could be that the IC can not drive the mosfet (IXTQ130N20T or IXFH400N075T2)?
The PCB was designed following the demo board.
All the gate signals seems correct but the one for the first mosfet has 3V and it should be 5V.
thanks in advance.
When you remove the MOSFET, does the Gate voltage become 5V?