Hi,
as per subject i'm looking for a reference design or spreadsheet to help to design a 50Vin (60 max) to 24Vout; 0.5A isolated power supply using LT8310 (or better). Operating loweer temp is -55°C
Any suggestion?
Thanks
LT8310
Production
The LT8310 is a simple-to-use resonant reset forward converter controller that drives the gate of a low side N-channel MOSFET from an internally regulated...
Datasheet
LT8310 on Analog.com
Hi,
as per subject i'm looking for a reference design or spreadsheet to help to design a 50Vin (60 max) to 24Vout; 0.5A isolated power supply using LT8310 (or better). Operating loweer temp is -55°C
Any suggestion?
Thanks
For -55 degree C operation, consider LT3748
Thanks very much. Can i use the same 1:1 transformer of the LT8304 also for the LT3748?
Mostly yes. Please use the equations in the LT3748 datasheet for double check.
Thanks very much
Is there any application note about flyback for application with the same input voltage range 18V to 80V and 48V output (approx 30W)?
Good starting point: