Post Go back to editing

ADP1613ARMZ-R7 Efficiency problem

Category: Software
Product Number: ADP1613ARMZ-R7

Hi there, 

Iam using your ADP1613ARMZ-R7 in the ADP1613 Step-Up Regulator Configuration

VOUT = 15 V
fSW = 650 kHz
VIN = 5V




When output current is around 200mA the input current is 700mA... 
Vin and Vout values are stable and correct. (5V and 15V)

efficiency = P_out / P_in = U_Out * I_out / (U_in * I_in) = 86%


Is there any way to reduce the input current ? 



Thank you so much in advance everyone! 

Regards!

Edit Notes

//Some errors in the post concept//
[edited by: Nasib.Fahim at 11:37 AM (GMT -4) on 2 Jun 2022]