Post Go back to editing

LTM4626/LTM4638 INTVcc

Category: Hardware
Product Number: LTM4626

It appears that the efficiency of LTM4626/LTM4638 is heavily affected by input voltage, supposedly due to the losses on internal LDO, generating INTVcc.

Is there a way of bootstrapping the INTVcc pin - from the output of the device itself, or from an external +3.3V power rail?

How the efficiency is affected?

Thanks in advance,

Parents
  • FormerMember
    FormerMember
on Jun 14, 2022 4:19 AM
0

Hello,

This is not possible as INTVCC is internally generated and an output pin, not an input.

Regards,

Jhun

Reply
  • FormerMember
    FormerMember
on Jun 14, 2022 4:19 AM
0

Hello,

This is not possible as INTVCC is internally generated and an output pin, not an input.

Regards,

Jhun

Children
No Data