Post Go back to editing

ADM1176 4 in parallel with different supply voltage

Category: Hardware
Product Number: ADM1176

I am using 4 ADM1176 one for +3V3, one for +5V and two for +12V
If I use +3V3 supply voltage for all of then or a combination of +3V3V and +5V for all of the, everything is working fine.
when I move to of them to +12V they disappears on the I2C bus.
It is the same set up, same IC, just the voltage there is change.
Any suggestion to why its not working 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.