Hi,
I've been working on a circuit that uses the LTC4366-2 as a surge and spike protection circuit. I designed the circuit simulation in the LTSpice with LTC4366-2. I have applied spike test within the ranges specified below.
I have used different MOSFET than simulation. Product number of MOSFET that I used is IPDQ60R010S7AXTMA1 in my application. The mosfet have 318nC total gate charge. I choosed value of total gate charge close to my MOSFET from LTSpice Library.
Also I have used two 120uF capacitor that ESR value is 1.47 ohm in source of MOSFET.
When I have run simulation, I saw 238V spike during 11us in simulation result and the design didn't make clamping straight. The simulation picture is below.
I think,
1) Could it be a problem, due to total gate charge of my mosfet ? If it is problem, How I can handle gate the problem with this mosfet?
2) Is important ESR value of capacitor for spike seen in output?
I shared circuit picture and LTSpice simulation file at the attachment.
gramer changes
[edited by: Baran at 10:52 PM (GMT -4) on 29 May 2022]