Post Go back to editing

LTC3779 OV shut down

Category: Hardware
Product Number: LTC3779

Hi,

I am using the LTC3779 in a high input voltage requirement of up to 145V. I would like to use the OV lock out feature to power down the part if the Vin exceeds 145V. Would there be any damage to the device if Vin exceeds 150V? The part will not turn on with the OV lock out above 145V but will there be any damage to the device if Vin exceeds 150V?

Thanks