Post Go back to editing

LT8210 Burn out the mosfet

Category: Software
Product Number: lt8210

Dear ADI:

    I use lt8210 for buck boost charger for battery , But now I use 2.5mΩ RSENSE series to inductor for sample inductor current , And my inductor saturation current about 30A , When input is 39V, output is 54.7V, LT8210 work in boost state and CCM mode ,Then the MOSFET A  and C  is burn out , Maybe Overcurrent  and inductor saturation, But i Check the datasheet page 5 about "Cycle-by-Cycle Inductor Current Limiting" ,The give message is that "VSNSP1 – VSNSN1 = 50mV"  If 50mV is correct , When I use 2.5mΩ Rsense , The Maximum current  just only 20A , I wanna know the VSNSP1 – VSNSN1= 50mV is right or not ,TKS!

Parents
  • Dear Chris: Now i have Fixed startup issues, But now i have find the problem as following:

          I use 4 mosfet, Every mosfet Qg about 50nC Then operation frequency is 200Khz, So i count out the current comsumption 

    I = 4*50nc*200K = 40mA, And external power 13V supply to EXTVCC and GATVCC about 10V ,When output current less than 0.5A/50.4V, GATVCC Ripple is very good, And LTC8210 efficient arrivate at 98.5% in CC mode, But if increase output current, For example 1A ,The lt8210's  GATVCC is very unstabity, So many problem is out, can you help me find out the reason

        I use external Switch Power IC power to EXTVCC pin ,can output 1A, When GATVCC unstabity, EXTVCC pin signal is very stablity

Reply
  • Dear Chris: Now i have Fixed startup issues, But now i have find the problem as following:

          I use 4 mosfet, Every mosfet Qg about 50nC Then operation frequency is 200Khz, So i count out the current comsumption 

    I = 4*50nc*200K = 40mA, And external power 13V supply to EXTVCC and GATVCC about 10V ,When output current less than 0.5A/50.4V, GATVCC Ripple is very good, And LTC8210 efficient arrivate at 98.5% in CC mode, But if increase output current, For example 1A ,The lt8210's  GATVCC is very unstabity, So many problem is out, can you help me find out the reason

        I use external Switch Power IC power to EXTVCC pin ,can output 1A, When GATVCC unstabity, EXTVCC pin signal is very stablity

Children
  • Hi fhlxUpdate,

    This sounds like the capacitor on either GateVCC or EXTVCC is to small. Try increasing the size of the capacitor.

  • hi cgass:

        Anther problem is that, The Internal GATVCC fault occured is easy ,For debug the board , I have used various MOSFET, But some mosfet cause the GATVCC output just 5V, Maybe it has some error, By the way, Can we short the ExtVcc and GATVCC?????

  •          Another problem when some chips GATVCC LDO have fault, Just output 3V to 5V,  No way for me, Cux ,All of sample chips have error, I just short GATVCC and EXTVCC, Strange phenomenon happened, boost and buck  is all work fine, But output voltage deviation about 3-5V, As the input gets higher and higher, the output deviates more and more! I can't understand the appearance,  The experience just as a test session,  But my mainly problem is how to protect GATVCC, If it's always have error when work with various Mosfet, Anyone have same prolblem with me ?

  • Hi fhlxUpdate,

    These are all new problems. I get very few questions on this part as it usually just works. Can you send your schematic and PCB layout? Gerber is fine.

    Did you get a demoboard and validate performance? It is good to have a demoboard as it is a reference you can compare.

    Thank you,

    Chris

  • Top layout

    inner for GND

    Inner for sigal

    bottom layout

    component and Top layer

  • PDF

    This sheet come from ADI Demo board 

  • Hi fhlxUpdate,

    The layout I think is OK. 

    I look at your schematic. You have a GATEVCC cap of 10uF and boost caps of 0.47 uF. Please check these values. If the ratio of GATEVCC cap to boost cap is not very high, then you can have difficulty getting a good GATEVCC voltage. As a rule of thumb, the GATEVCC cap should be 100x the boost cap. Please check to make sure that you have adequate GATEVCC capacitance.

    Thank you,

    Chris

  • Hi  cgass, Very thankful you at least, I Try to add GATEVCC caps to 20uF, But no good effect In large current, Cux PCB's room limited, Big caps can't add, So stop! I have designed LT87xx series Chips etc, just GATEVCC is 10 times is okey, For Lt8210, gateVCC is so high, maybe Capacitor is high too.

    In fact, I have Test 5 PCS board, First 54V/2A output , Efficiency is very good, But my project At least  400W and more!As the current increases, the MOSFET suddenly burn, and then GATVCC is Abnormal next times!!! Now expect new Sample IC for prototype, Tks you any ways

  • You can also reduce the boost cap value to 0.1uF. Either increase GATEVCC or reduce boost.

  • Dear cgass: my Project requirement about 500W power supply, If  boost cap value to 0.1uF, Just only use lower Qg value Mosfet, Isn't it ? Low Qg valuce MOSFET Rdson is high, And the very hot, And discrease the efficient? 

      Another problem, GATVCC capacitor size is increase, and output is stablity, And can work in  400W output, But Inner LDO Get issue, Very easy break; especially startup, Damage to LDO due to transient inrush current When high caps!Maybe Series limiting resistor can do it ,I have Broken 8 pcs chips Since the LDO can't work, Maybe high power output for LT8210 is not good