KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
LTC3786
Production
The LTC3786 is a high performance synchronous boost converter controller that drives all N-channel power MOSFETs. Synchronous rectification increases efficiency...
Datasheet
LTC3786 on Analog.com



Circuit is as shown, very similar to the default boost converter. Input voltage is from a battery or DC supply, ranges from 10 to 19V, with 24V output. The scope images show the regulated 24V output on Ch1, and Ch2 is the ITH pin. The load is a BLDC motor that can change direction but is driven via a trapezoidal move profile. The spike is on a stop, just before a direction change. I might assume that the ITH is showing me the device is going to sleep, so the MOSFET devices are both OFF. Is this expected behavior? Is there a way to configure the 3786 to reduce the output voltage so that my peak ripple is significantly less?