KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC3786
Production
The LTC3786 is a high performance synchronous boost converter controller that drives all N-channel power MOSFETs. Synchronous rectification increases efficiency...
Datasheet
LTC3786 on Analog.com



Circuit is as shown, very similar to the default boost converter. Input voltage is from a battery or DC supply, ranges from 10 to 19V, with 24V output. The scope images show the regulated 24V output on Ch1, and Ch2 is the ITH pin. The load is a BLDC motor that can change direction but is driven via a trapezoidal move profile. The spike is on a stop, just before a direction change. I might assume that the ITH is showing me the device is going to sleep, so the MOSFET devices are both OFF. Is this expected behavior? Is there a way to configure the 3786 to reduce the output voltage so that my peak ripple is significantly less?
It looks like the motor is bumping the Vout up above the output set-point which would result in ITH pin pulling low (that would stop switching). The input voltage may also go up in this case since the current could flow from Vout to Vin. It may be helpful to look at the Vin and RUN pin levels as well.