Post Go back to editing

LTC4417 Droop

Category: Hardware
Product Number: LTC4417

Hi,

The load is 66-120W and this could be 3.5 to 13.89Amps. It has a voltage range of 8V98-18V11.

I am using the LTC4417 PowerPath Controller Design Tool to design three power sources.

beta-tools.analog.com/.../

The tool suggests a 26V9 droop could occur.

The load has a 8V98 minimum.

Does this mean that if channel 2 falls to 9V, it will then droop by up to 26V9 while switching to channel 3?

If this is correct, this will cause the load to power down.

Increasing the output capacitance in the tool does not help. Are there any suggestions to solve the droop problem?

I will try LTspice

Parents Reply
  • Thanks for the support. The LTSPice model seems more accurate and does not show the same droop. I modelled the input stage of the load and was able to iteratively adjust the slew rate to keep within the current limits. I also adjusted the UV & OV resistors to keep the droop within the load limits.

Children
No Data