Does the LTM4607 support direct parallel connection? Can two LTM4607 output directly in parallel? Do you need to add ltc6908-1 synchronization?
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Awaiting Customer Response | |
LTM4607
Recommended for New Designs
The LTM4607 is a high efficiency switching mode buck-boost power supply. Included in the package are the switching controller, power FETs, and support...
Datasheet
LTM4607 on Analog.com
LTC6908-1
Production
The LTC6908 is an easy-to-use precision oscillator that provides 2-outputs, shifted by either 180° or 90°. The oscillator frequency is programmed by...
Datasheet
LTC6908-1 on Analog.com
Does the LTM4607 support direct parallel connection? Can two LTM4607 output directly in parallel? Do you need to add ltc6908-1 synchronization?
Does the LTM4607 support direct parallel connection? Can two LTM4607 output directly in parallel? Do you need to add ltc6908-1 synchronization?
Does the LTM4607 support direct parallel connection? Can two LTM4607 output directly in parallel? Do you need to add ltc6908-1 synchronization?
Hi Clark666,
Fig. 20 typical application is best way to go. This is a proven and tested circuit. Recommended to use LTC6908-1. Thanks.