Hi,
I have a few questions in regards to using the LT3092
1 - I see that the maximum junction temperature specified on this part is 125C but in the datasheet's performance characteristic graphs, it has data that goes to 150C. The datasheet also states the the part will thermally shut off at 125C. If this is the case then why does the datasheet show performance characteristic graphs go up to 150C
2 - I plan to use this part in a high voltage application. Looking at the application circuits, it seems like that we can put the LT3092 in series to increase the operating voltage. Is there any limitations on how many of them can be put in series? I am thinking that i may have to put 5 of them in series to meet my voltage spec.
3 - I will have to decrease the power dissipation in the LT3092 with the extra resistor across Vin and Vout as per the application circuit. Will this have any effect on putting multiple LT3092 in series?
Thanks