Post Go back to editing

DCDC converter with dual supply

Category: Software
Product Number: DCDC converter with dual supply

Hi,

May I know if ADI has any similar component for LTC3260?

Was thinking whether the LTC3265 can be used as an alternative solution as LTC3260..

Input 24V, output >±12V

Thanks. 

Edit Notes

Alternative
[edited by: Clt at 4:31 AM (GMT -4) on 17 May 2022]

Hello,

You won't be able to use the LTC3265 as its input supply is only rated up to 16V for VIn_P. Is your input fixed at 24V?

  • Hi Jhun,

    Thanks for your prompt response.

    Yes the current voltage input is fixed at 24V. 

  • Hi Clt,

    LTC3265 has a boost charge pump which only has a max input of 16V. It also means you cannot produce a stepped down +12V output.

    However, the inverting charge pump can take 24V input and produce -12V output through the negative LDO.

    You can try looking for charge pumps from this table: Selection Table for Inductorless (Charge Pump) DC/DC Converters | Parametric Search | Analog Devices

    You can also look into LTM4655 which can operate within your desired specs: LTM4655 Datasheet and Product Info | Analog Devices