Hello,
I need a regulator (buck boost?) that can handle an input voltage of at least 3-8.4V. Currently, the input will be one LiPo cell (3.7V) but might become two in series (7.4V) in the future. It is used to drive 3 BDC motors. Generally, the motors can draw up to 2.5A together but I have seen short bursts >4A. The output voltage should be able to be at least 6V. Do you have any recommendations? (I came across the LTC3785EUF-1 myself. Looks like something like that may work?)