I get this question relatively frequently these days so I will post the question and then answer it myself in another post:
What are the requirements for COUT so the LT1764 linear regulator and similar LT176X LDOs are stable?
LT1764
Production
The LT1764 is a low dropout regulator optimized for fast transient response. The device is capable of supplying 3A of output current with a dropout voltage...
Datasheet
LT1764 on Analog.com
LT1761
Recommended for New Designs
The LT1761 series are micropower, low noise, low dropout regulators. With an external 0.01µF bypass capacitor, output noise drops to 20µVRMS over a 10Hz...
Datasheet
LT1761 on Analog.com
LT1762
Recommended for New Designs
The LT1762 series are micropower, low noise, low
dropout regulators. The devices are capable of supplying
150mA of output current with a dropout voltage...
Datasheet
LT1762 on Analog.com
LT1763
Recommended for New Designs
The LT1763 series are micropower, low noise, low dropout regulators. The devices are capable of supplying 500mA of output current with a dropout voltage...
Datasheet
LT1763 on Analog.com
I get this question relatively frequently these days so I will post the question and then answer it myself in another post:
What are the requirements for COUT so the LT1764 linear regulator and similar LT176X LDOs are stable?