I get this question relatively frequently these days so I will post the question and then answer it myself in another post:
What are the requirements for COUT so the LT1764 linear regulator and similar LT176X LDOs are stable?
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT1764
Production
The LT1764 is a low dropout regulator optimized for fast transient response. The device is capable of supplying 3A of output current with a dropout voltage...
Datasheet
LT1764 on Analog.com
LT1761
Recommended for New Designs
The LT1761 series are micropower, low noise, low dropout regulators. With an external 0.01μF bypass capacitor, output noise drops to 20μVRMS over a 10Hz...
Datasheet
LT1761 on Analog.com
LT1762
Recommended for New Designs
The LT1762 series are micropower, low noise, low
dropout regulators. The devices are capable of supplying
150mA of output current with a dropout voltage...
Datasheet
LT1762 on Analog.com
LT1763
Recommended for New Designs
The LT1763 series are micropower, low noise, low dropout regulators. The devices are capable of supplying 500mA of output current with a dropout voltage...
Datasheet
LT1763 on Analog.com
I get this question relatively frequently these days so I will post the question and then answer it myself in another post:
What are the requirements for COUT so the LT1764 linear regulator and similar LT176X LDOs are stable?
My perception is that the LT1764 and similar LDOs require ESR for stability in general BUT those LDOs were designed when the typical COUT was tantalum and not ceramic, PLUS tantalum capacitors at that time had higher ESR than typical tantalum and polymer capacitor have now, so now LT1764 circuits can have stability problems because customers want to either use ceramics for COUT or modern low ESR tantalums or polymers that don’t have enough ESR either.
Further, the LT1764 datasheet does not do a good job explaining how much COUT ESR is necessary for stability.
I recommend that customers consider the guidance in the LT1764A datasheet about COUT and ESR. The LT1764 and LT1764A probably do have a subtle feedback loop difference, but it is also important that the LT1764A datasheet does a much better job characterizing the LT1764A (and probably the LT1764) stability based on VOUT, COUT and COUT ESR. The LT1764A datasheet specifically mentions that it may be necessary to add ESR outside of the chosen COUTs. I show that text in the image below:

You can see that the LT1764 is sensitive to COUT ESR just using LTspice. I uploaded my evaluation circuit. But it is best if customers perform a load transient test on their hardware and make sure they have some margin to prevent instability due to part-to-part or temperature variation.
Lastly, the LT1764 and similar LDOs are also sensitive to the amount of CIN depending on the input power network, but the datasheets do not mention that either. Make sure CIN is sufficient for your circuit and include some margin for part-to-part and temperature variation.