Post Go back to editing

LTM8024 (DC1868A) small voltage dip after startup

Category: Hardware
Product Number: LTM8024

I'm DFAE in Japan.

My customer start evaluating LTM8024 using DC1868A in the force continuous mode operation.

He uses DC1868A with JP1 setting to NON BURST.

He found the small dips(about 100mV) in both 5V and 3,3V  regulated output after the start up.

Would you inform me what happened and how can he fix this problem?

I attach the oscilloscope shot(green is VIN, yellow is 5V output, blue is 3.3V output)

Parents Reply Children
  • Hello Chaz,

    Glad to see this thread already exists because I am having the same observations.
    Burst mode helps for some reason, but that's non-intuitive. I would think that Forced CCM would keep the top FET switching thus preventing this issue, whilst Burst Mode *could* allow for skipped switching cycles that may materialize into the observed dips.

    If you have any additional insight, please share.

    Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.