Post Go back to editing

LTC4366 with parallel FETs?

Thread Summary

The user is designing a circuit with the LTC4366 and is considering using two FETs in parallel to meet SOA needs during surges. The final answer confirms that the LTC4366 can drive two FETs in parallel, which will naturally balance current during normal operation. A low Qg FET is recommended to reduce the driving load on the IC. The control loop should handle multiple FETs without leading to instability, but tight regulation during surges is not guaranteed.
AI Generated Content
Category: Hardware
Product Number: LTC4366

I'm designing a new circuit with the LTC4366 and having trouble finding a suitable, in-stock FET that can meet my SOA needs during a surge.  Is it possible to use two FETs in parallel with this device?  During normal (non-surge) operation will they naturally balance current based on heating?  During surges will the control loop for the 4366 be able to handle multiple FETs or will it lead to instability?  I'm not too concerned with having tight regulation during a surge. 

  • Hi Ryan,

    LTC4366 should be able to drive two FETs in parallel. Pick a low Qg FET to lower the load for the IC to drive since you're driving multiple MOSFETs.

    During normal (non-surge) operation will they naturally balance current based on heating? 

    Yes. This is correct. As long as you follow the datasheet recommendation, this should be fine.

    Regards,

    Jhun