Category: Hardware
Product Number: LTC3307A
Hello,
Three questions:
LTC3307A is a buck converter and is specified as a 5V, 3A part.
1. Does it mean it can deliver 15W of Pout?
At another part in the Datasheet, a ref design shows output as 1.2V @3A
2. Does it mean its output power is 3.6W?
I have used it as a buck going from 5V to 3V.
As part of my analysis, I need to hit Vin with a voltage higher than its Absolute Maximum Value, which is 6V.
In LTspice, I have used a PWL source as Vin, which starts at 5V and later it hits 10V.
After simulation, no change happens, i.e. Vin =10V & Vout =3V.
3. Does it mean the part can work when Vin = 10V?
Thank you,
Ray