Post Go back to editing

POE dominance and seamless transistion from AUX to POE: is it possible with LTC4278 ?

Thread Summary

The user asks about achieving PoE dominance with the LTC4278 and the behavior when using both a 12V wall adapter and PoE. The final answer confirms the behavior: if PoE is connected first, it will supply power and transition seamlessly to the adapter if PoE is removed. If the adapter is connected first, PoE detection/negotiation will not start, and there will be no seamless transition to PoE if the adapter is removed. The user also inquires about the possibility of a seamless transition from the adapter to PoE, but no solution is provided.
AI Generated Content
Category: Hardware
Product Number: LTC4278

any schematics example ?