Hi Sir,
I got the ADP5588 application information at the link below,
RE: AD5588 Vcc maximum operating voltage
So, I would like the confirm with you that,
That means all pins(VCC, R0..R7, C0...C9, SCL/SDA, RST* and INT*) can operate at 3.3V and work fine, right?
And if the pin is not used (Rx or Cx), could it be pulled to the VCC voltage with a resistor?
Thanks.