Hi, everybody,
I am trying to understand if the LT8228 can be used in my application:
I have an input Voltage of 12V (to say at the V1 input of the LT8228 reference circuit) and I have to charge a supercapacitor bank: 4 strips in series producing a maximum voltage of 10.8V, with a limited current of 20A.
Now the question is: Is the buck section of the LT8228 capable to work at 12V input and producing a max 10.8V@20A at the output?
Best regards.
Maurizio