Post Go back to editing

Handling of unused pins of LTC3315A

Hello

When using the output of LTC3315A with only 1ch, how should the following pins be processed?

・ Unused terminal
3: FB2
4: EN2
6: SW2
7: VIN

I would appreciate it if you could reply.

Best Regards,
Knj

  • Hello,

    The unused EN and FB should not float and should connect to GND. The VIN pin that supplies the unused regulator is still connected to VIN internally. This pin should connect to VIN and have a decoupling cap on it. A smaller decoupling cap like 0.1uF to 1uf can can be used close to the pin. The bigger bulk cap can be close to the regulator in use. The unused SW node should float.