Hi,
When using one (1) LTM4675 and not using its SHARE_CLK function, is it OK to leave the SHARE_CLK pin Open?
Also, is there any setting when using one (1) LTM4675?
Regards,
Kazu
LTM4675
Recommended for New Designs
The LTM4675 is a dual 9A or single 18A step-down μModule® (micromodule) DC/DC regulator with 40ms turn-on time. It features remote configurability and...
Datasheet
LTM4675 on Analog.com
Hi,
When using one (1) LTM4675 and not using its SHARE_CLK function, is it OK to leave the SHARE_CLK pin Open?
Also, is there any setting when using one (1) LTM4675?
Regards,
Kazu
Hi Kazu,
Yes you can leave the pin open.
For your question two, you can see figure 34 on page 76 on the datasheet. You can also verify your design using LTSpice.
Regards,
Jhun