Post Go back to editing

ADP5350 battery charging issue

Hi,

Result from our charge test shows that battery level increases linearly during the charge.

See the image below for charge graph:

- X axis is time in hour.

- Battery level is read from ADP5350 chip.

Schematic

Configuration

Register Name Address Value Register Name Address Value
Manufacture and model ID 0x00 0x1B K_RBAT_CHARGE 0x1F 0x01
Silicon revision 0x01 0x03 BAT_TEMP 0x20 0x5B
CHARGER_VBUS_ILIM 0x02 0x0A BAT_SOC 0x21 0x09
CHARGER_TERMINATION_SETTINGS 0x03 0xAC VBAT_READ_H 0x22 0x83
CHARGER_CURRENT_SETTING 0x04 0x3E VBAT_READ_L 0x23 0xF8
CHARGER_VOLTAGE_THRESHOLD 0x05 0x5B FUEL_GAUGE_MODE 0x24 0x01
CHARGER_TIMER_SETTING 0x06 0x78 SOC_RESET 0x25 0x00
CHARGER_FUNCTION_SETTING1 0x07 0xCF BST_LED_CTRL 0x26 0x1C
CHARGER_STATUS1 0x08 0x02 BST_CFG 0x27 0x00
CHARGER_STATUS2 0x09 0xE4 IBL_SET 0x28 0x00
CHARGER_FAULT 0x0A 0x00 ILED2_SET 0x29 0x00
BATTERY_SHORT 0x0B 0x45 ILED3_SET 0x2A 0x00
BATTERY_THERMISTOR_CONTROL 0x0C 0x38 ILED4_SET 0x2B 0x00
V_SOC_0 0x0D 0x6B ILED5_SET 0x2C 0x06
V_SOC_5 0x0E 0x8E BL_FR 0x2D 0xDD
V_SOC_11 0x0F 0x92 LED3_BLINK 0x2E 0xB4
V_SOC_19 0x10 0x97 LED4_Blink 0x2F 0xB4
V_SOC_28 0x11 0x9A LED5_Blink 0x30 0xB4
V_SOC_41 0x12 0xA4 LED_STATUS 0x31 0x00
V_SOC_55 0x13 0xAE LDO_CTRL 0x32 0x07
V_SOC_69 0x14 0xB8 LDO_CFG 0x33 0x00
V_SOC_84 0x15 0xCE VID_LDO12 0x34 0x92
V_SOC_100 0x16 0xD4 VID_LDO3 0x35 0x02
FILTER_SETTING1 0x17 0x44 PGOOD_STATUS 0x36 0x0D
FILTER_SETTING2 0x18 0x00 PGOOD_MASK 0x37 0x08
RBAT_0 0x19 0x3F CHARGER_INTERRUPT_ENABLE 0x38 0x00
RBAT_10 0x1A 0x3F CHARGER_INTERRUPT_FLAG 0x39 0x00
RBAT_20 0x1B 0x3F BOOST_LDO_INTERRUPT_ENABLE 0x3A 0x00
RBAT_30 0x1C 0x3F BOOST_LDO_INTERRUPT_FLAG 0x3B 0x00
RBAT_40 0x1D 0x3F DEFAULT_SET 0x3C 0x00
RBAT_60 0x1E 0x3F NTC47K_SET 0x3D 0x01

Battery profile

/cfs-file/__key/communityserver-discussions-components-files/330/PCNV553037_2D00_750mAh-1-_2D00_-en.xlsx

/cfs-file/__key/communityserver-discussions-components-files/330/PCNV553037_2D00_750mAh-2-_2D00_-en.xlsx

Please help to check whether I am using the chip correctly.

Thanks.

Parents Reply Children
No Data