Post Go back to editing

LT3932 minimum current when use CTRL pin

Hi all

We want to use LT3932 to design our circuit with parameter below

1. input: 24VDC

2. output (LED): constant current from 5mA to 1200mA

so, without using external PMOS and PWM pin, only control CTRL PIN by PWM signal, could i adjust output current from 1200mA to 5mA. I think 5mA is so small

Parents
  • Hi phamtrieu138,

    Based on page 14 of the datasheet, the LED current can go to zero for duty cycle of less than 12.5%. I think 5mA can be achieved.

  • 1. with output current = 1.2A max, Rsense = 0.082 ohm.

    2. with Rsense = 0.082 ohm, Ioutmin = 5mA, Isp-Isn = 0.41 mV.  This voltage is more than offset voltage of a lot of amplifiers. In datasheet, i don't see the offset voltage of inside amplifier of output current sense module. so, could you tell me this parameter?

  • Hi phamtrieu138,

    I consulted with product expert and I would like to correct my answer. This is not exactly possible (at least with a single LED driver). The offset voltage for the current sense amplifier becomes an issue at that low of a differential sense voltage. For an application like this that requires such a wide range of analog dimming, you would need two LED drivers to perform this function with any sort of accuracy. It would allow for a bit better optimization of the lower current level accuracy but requires a bit of control logic to send the analog dimming signals to each converter and have smooth transitions between coarse and fine adjustments. 

Reply
  • Hi phamtrieu138,

    I consulted with product expert and I would like to correct my answer. This is not exactly possible (at least with a single LED driver). The offset voltage for the current sense amplifier becomes an issue at that low of a differential sense voltage. For an application like this that requires such a wide range of analog dimming, you would need two LED drivers to perform this function with any sort of accuracy. It would allow for a bit better optimization of the lower current level accuracy but requires a bit of control logic to send the analog dimming signals to each converter and have smooth transitions between coarse and fine adjustments. 

Children