LTM4686
Recommended for New Designs
The LTM4686 is a dual 10A (12A Peak) or single 20A (24A Peak) step-down µModule® (micromodule) DC/DC regulator with 39ms turn-on time. It features remote...
Datasheet
LTM4686 on Analog.com
I want to replace an obsolete Intersil part with the LTM4686 (single output configuration) and I would like to design the replacement to use either LTM4686 or LTM4686-1 with 12V VIN.
It seems from the datasheet I can just add a separate 5V LDO to supply INTVCC with either part, and have 0ohm's to connect SVIN to VIN for the 4686 and SVIN to INTVCC for the 4868-1. Is this correct?