Post Go back to editing

About the waveform at the start of LTC4413

Hi,

I have a question.
Please give me an answer.

Please tell me about the startup waveform of LTC4413.
During the experiment, the output flutters around 2.5V.
(See the waveform below)
Is this normal behavior?

If it works normally,
Please tell me the worst fluttering time and fluttering amount.

※INA:0V(No DCDC output) ENBA:0V(Low)

(circuit diagram)

※The LDO output is being input to the INB.

Best Regards,

Naohisa

Parents
  • Hi Naohisa,
    What kind of load do you have on OUTA/B?

    On page 8 in the datasheet:
    "The LTC4413-1 (or LTC4413-2) is recommended for
    applications with demanding load step or fast slew rate
    requirements. The LTC4413-1 and LTC4413-2 provide better
    load regulation in these environments at the expense
    of higher quiescent current. The LTC4413 is optimized
    for lower power consumption and should not be used in
    high slew rate environments or when large and fast load
    transients are anticipated."

    The -1 or -2 version may resolve your issue.

    -Aaron

Reply
  • Hi Naohisa,
    What kind of load do you have on OUTA/B?

    On page 8 in the datasheet:
    "The LTC4413-1 (or LTC4413-2) is recommended for
    applications with demanding load step or fast slew rate
    requirements. The LTC4413-1 and LTC4413-2 provide better
    load regulation in these environments at the expense
    of higher quiescent current. The LTC4413 is optimized
    for lower power consumption and should not be used in
    high slew rate environments or when large and fast load
    transients are anticipated."

    The -1 or -2 version may resolve your issue.

    -Aaron

Children
  • Hi Aaron,

    thank you for your answer.


    Nothing is connected to OUTA.
    SATA-connected SSD (before booting), SD card (before booting), Buffer-IC, and several logic ICs are connected to OUTB.

    By the way, there is no change in the waveform even if SSD and SD card are not connected (load is only a few logic ICs).

    After all, is the slew rate too high?

    For LTC4413 not of -1, -2
    Is this phenomenon at startup normal?

    Do you know the range of error (time and voltage) in that case?

    Because I don't have time to change the design
    There is no choice but to use LTC4413.

    Best Regards,

    Naohisa

  • Is this phenomenon at startup normal?

    I used the LTC4413 demoboard (DC839A), and applied the same 3.3V input with a 50V/ms slew rate. No load.

    OUT waveform looks similar to what you saw.

    Here is the same scopeshot, but with the -2 version:

    Once IN reaches 3.3V, OUT came up 50us quicker for the -2 version.

    Do you know the range of error (time and voltage) in that case?

    I don't see that spec in the datasheet. Sorry.

    Because I don't have time to change the design
    There is no choice but to use LTC4413

    The -1 and -2 version should have the same pinout, so minimal changes.

    -Aaron

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.